This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: IWR1443

Part Number: IWR1443

I can flash program to IWR1443 on Circuit board produced.But IWR1443 boot up,but it stop working at once. 

I can flash program to IWR1443 on EVM(IWR1443Boost), IWR1443 work normal. I use xwr14xx_high_accuracy_mss to flash.

VOUT_14SYNTH is 1.42V 、VOUT_PA1 is 1V、VOUT_PA2 is 1V on EVM(IWR1443Boost).but VOUT_14SYNTH is 0V 、VOUT_PA1 is 0V(No R13)、VOUT_PA2 is 0V(No R13) on on Circuit board produced.

4201.IRW1443.pdf