This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP116: data retention time over temperature

Part Number: TMP116

Hi,

we want to use the temperature Sensor TMP116N in one of our designs.
According to the data sheet, it has a specified data retention time of min. 10years, typ. 100years.
We need a data retention time of min. 20y at an operating temperature of -40 to + 85 ° C.
Are there any diagrams  that shows the behavior over the temperature range? Or any other additional information?

Thanks for your support.

Alen

  • Hi Alen,

    The minimum spec of 10 years is inclusive: -55C to 125C and 1.9V to 5.5V. The typical spec of 100 years is only for 25C and 3.3V. Since your requirements are less than the extremes, we can expect more than the 10 year minimum in your application. However, this is all the guidance we can provide. We don't have additional data to share.

    thanks,

    ren