Hi,
Good day. I hope you are doing fine there.
Our customer wants to know if we have a graph that shows the OPT101 Responsivity vs Temperature. For example, if TA = 25 °C and other condition is Ta =30 °C then would the temperature will have an effect to the device responsivity/performance?
In addition, the customer is using the OPT101 to detect a laser light pulse. they want to understand that if the received light on OPT101 surface will increase photo diode temp or not?
I would appreciate if you could help us provide this information.
Thank you and always keep safe.
Regards,
Cedrick