Other Parts Discussed in Thread: HDC2080, HDC2021
Hi
I am currently using the HDC1080 and would like to know the following so i can optimise the best way of using it?
1. What is the purpose or correct way to use the heater? Is there away on power up to detect the necessity of heater ? Under what circumstance would we need to use it?
2. There is RST bit in the configuration what is the purpose of it?
3. Once a minute i am reading temperature/humidity sample. Is once sample reading enough, or should i be reading it multiple times within that minute for an average?
As the output is digital data, i though averaging might not be necessary?
4. Can the size of GND plane or GND pour have any effect on the results. At times two device next to each other would have few degrees for temperature or % for humidity difference. Is this acceptable? If one the PCB is charging a PCB the sensor does show about 5-6 degree extra on that.
5. I manually soldered the IC using hot air, i then cleaned the board to remove all the flux. Can this effect the readings?
Thank You
Regards
DJ