Part Number: OPT3002
Hi,
My customer want to use OPT3002, but the application has different I/O voltage from VDD as shown in below. Is that no problem? The logic HIGH input voltage (V_IH) is described as 0.7*VDD(min.) to 5.5V(max.) according to the datasheet.
Customer's application:
VDD: 3.3V
I/O: 1.8V
I/F:I2C-Fast(400kHz)
No proximity sensor
Best Regards,
Kazuto