HI,
The maximum output at Extended mode = 0 is 127.9375 degree C (0x07FF). Will the output keep the value when temperature rise over 127.9375 degree C?
Regards,
Nagata.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI,
The maximum output at Extended mode = 0 is 127.9375 degree C (0x07FF). Will the output keep the value when temperature rise over 127.9375 degree C?
Regards,
Nagata.
Hi Nagata,
Yes the value will stay at 0x7FF if the device in Extended Mode = 0 and temperature rises above 127.9375 °C.
Thanks,
David