For pin P13, SPI_HOST_INTR. If we config the spi as slave mode, do we need to toggle SPI_HOST_INTR manually to notify the host that data is available ?
Or it will be handled magically via the SPI_transfer function ?
If we need to toggle manually , how ? since it is not gpio mode, it had a dedicated mode.
#define SOC_XWR68XX_PINP13_PADAA 0U
#define SOC_XWR68XX_PINP13_PADAA_GPIO_12 0U /*< General Purpose IO*/
#define SOC_XWR68XX_PINP13_PADAA_SPI_HOST_INTR 1U /*< General Purpose IO*/
#define SOC_XWR68XX_PINP13_PADAA_SPIB_CSN1 6U /*< SPI Channel B Chip Select*/