We are currently using the AWR1642 with the web visualizer, at the best range configuration. Whenever we send the MAX radial velocity parameter to be above 8m/s, the sensor will go to a non-usable state and the visualizer will freeze up. We will have to unplug the sensor and plug it back in to get it back to a usable state. We've also seen it freeze up when the setting was set to about 4m/s. Why is this happening, and how can we stop this from happening? Thanks for the help.