Other Parts Discussed in Thread: TM4C1294NCPDT
Tool/software: Code Composer Studio
Hi,
I'm trying to reproduce the Out of Box Demo using the IWR1642BOOST EVM board following the guide http://dev.ti.com/tirex/content/mmwave_industrial_toolbox_4_2_1/labs/out_of_box_demo/16xx_mmwave_sdk/mmw_16xx_user_guide.pdf provided by the TI Resource Explorer under Industrial Toolbox 4.2.1.
I'm stuck at the point 5.1 in which the EVM should be connected to the CCS.
I'm using the CCS v10 and mmWave SDK 2.0.0.4 as suggested by the guide and they are running inside a VM with Ubuntu 16.04.2 LTS as OS.
I was trying to test the connection of a new .ccxml configuration file, when it had raised an error concerning the firmware update of the EVM.
I got that the tool turned the EVM in DFU mode but in this way the EVM was disconnected and since it was running inside a VM it did not connect automatically the usb ports.Before understanding that I had to connect the EVM in firmware updating mode from USB tool of virtualbox I tried to use also xdsdfu command line program.
I've tried to use the xdsdfu tool in a terminal shell loading the firmware directly (firmware_3_x_x.bin) and it raised an error.
For this reason, finally I've also tried to load the bootloader binary present in the directory but after power cycling the EVM I was no more able to see the ports.
At this point I tried power cycling several times the EVM but I didn't see anymore the ports under the OS X host under which the virtualbox VM was running.
Is it possible that the bootloader bin of the xdsdfu tool has kind of broken something ? Is there any kind of hardware hard reset to solve this kind of problem ?
Best regards
Trex