The datasheet discusses repeatability for averaging vs not-averaging the results.
The datasheet lists LSB as 0.0078℃, or 7.8m℃
Then 7.3.2 discusses this difference of averaging, stating that:
As shown in the noise histograms of Figure 6 and Figure 7, the temperature result output has a repeatability of approximately ±3 LSBs when there is no averaging and ±1 LSB when the device is configured to perform eight averages.
But looking at these graphs, the distribution is over ±70m℃...which is ±10LSB given that 1LSB is 7.8m℃
I think this is a problem with the datasheet. Please confirm.
Regards,
Darren