Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR6843
Team,
-Is there a way to do "pseudo real-time"processing with IWR1642BOOST + DCA1000 and Matlab?
What I mean is acquire raw data with the IWR1642BOOST + DAC1000, read it on the fly and process it in Matlab.
So far customer could only achieve post-processing (ie record the raw data and then process it)
-I understand that for this scenario the throughput/bandwidth might be limited and that it could reduce the frame rate.
But Is it possible at all?
-I have seen some some python scripts (see e2e post here) are available for the PC side to talk to the IWR1642BOOST via the UART.
Are there some Python modules that would enable to talk to the DCA1000 and interface to matlab in order to stream raw data?
Thanks in advance,
A.