This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP513: Center Pad Vias Required

Part Number: TMP513

I saw in the related question that the QFN pad should be connected to ground. I had the same question, as it is not mentioned in the datasheet (maybe worth updating the datasheet to mention this?). Ok, so I'm connecting it to ground at least by connecting to pin 14. However, does this center pad also need in-pad vias to connect to the ground plane beneath this chip? I assume this chip doesn't require that from a thermal perspective, but does it help with noise performance on the ADC?

  • The thermal pad can be connected to GND or left floating. It doesn't require vias. You're correct that it doesn't need the via material to conduct heat away from the chip as it does not have high current consumption. The ADC is not affected by the thermal pad, either.

    thanks,

    ren