hi
I am testing by connecting opt3101 to the NRF52810 project by I2C method, but the distance data is strange.
Can I get a demo source file?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi
I am testing by connecting opt3101 to the NRF52810 project by I2C method, but the distance data is strange.
Can I get a demo source file?
Hi,
OPT3101 is not plug and play as there is a calibration/configuration needed so want to make sure you are not just powering up without calibration as then distance data will be wrong. All this is done on the EVM but if you are using a custom board or doing something else want to make sure this is taken care of. We have a number of resources for this device to help. The SDK would the be demo code that allows you to run calibration and read data.
All can be found here https://e2e.ti.com/support/sensors/f/1023/t/815766
Best,
Alex