Other Parts Discussed in Thread: MMWCAS-RF-EVM, AWR1443, AWR2243
I have questions about AWR1443BOOST.
1) Using two AWR1443BOOST units, the signal transmitted from the first unit is received by the second unit and the waveform of the FM-CW radar transmitted from the transmitting side is sent to the other unit using RSSI (IQ signal)
Is it possible to use it in the form of reading as? (To measure the relative transmission level in the space of 80 GHz band).
At that time, we are thinking of making the transmission signal of the second unit invisible by an electromagnetic wave absorber.
2) Is it possible to control two units of AWR1443BOOST with one PC using the first SPI as master and the second module SPI as slave?
3) If 1) and 2) cannot be done with AWR1443BOOST, is it possible with cascade type AWR1243P (as a board MMWCAS-RF-EVM)?
Thank you.