Good evening,
I'm working on a project regarding current detection.
The target is to know if there is a DC current flowing in an electrical cable. I just need a binary answer, for example, I > 1A => switch out high; I < 1A => switch out low. The output of the switch will be used as a trigger for another device.
The current could vary from 3A to 1200A and the cable width vary from 5mm to 50mm.
I think a hall switch can be used for this purpose, but I didn't understand how to place it near the cable and if there is a sensor that is capable to detect a current of about 5A.
In addition, the switching behaviour should be fast, order of microsec.
Thanks in advance.
Best regards,
Lorenzo.