Recently, I encountered a problem in debugging 1243. I can implement 150m MIMO and 300m BF tests separately.However, I want to use cascade 1243 to realize the target detection in both the short and long distance at the same time. I use MIMO and BF methods in 3.8 processor_ SDK_ RADAR_ 03_ 08_ 00_ No related demo was found in the SDK of. Do you know if it can be implemented? Please let me know. Thank you