Hi Team,
When the temperature is 50 degrees, the output voltage center point voltage has a drift of 100mV compared with 25 degrees. But after the temperature returns to 25 degrees, the center point of the output voltage does not return to the original value at 25 degrees. And it needs to be completely powered off and then reconnected to restore the value corresponding to 25 degrees. Customer would like to know how to resolve this issue?
Thanks,
Annie