Hi
I used the SensingMMwaveEstimator to get a profileCfg and frameCfg for the mmwave sensor. I added this to an existing configuration, which gives me a 3D pointcloud with the ROS example. I just changed the profileCfg and frameCfg, however it seems like the outpus changed to 2D.
The configuration is
sensorStop flushCfg dfeDataOutputMode 1 channelCfg 15 7 0 adcCfg 2 1 adcbufCfg -1 0 1 1 1 profileCfg 0 77 2 3.9 19.85 0 0 49.97 1 166 11104 0 0 30 chirpCfg 0 0 0 0 0 0 0 1 chirpCfg 1 1 0 0 0 0 0 4 chirpCfg 2 2 0 0 0 0 0 2 frameCfg 0 0 53 0 100 1 0 lowPower 0 0 guiMonitor -1 1 1 0 0 0 1 cfarCfg -1 0 2 8 4 3 0 13 0 cfarCfg -1 1 0 4 2 3 1 11 0 multiObjBeamForming -1 1 0.5 clutterRemoval -1 0 calibDcRangeSig -1 0 -5 8 256 extendedMaxVelocity -1 0 lvdsStreamCfg -1 0 0 0 compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 measureRangeBiasAndRxChanPhase 0 1.5 0.2 CQRxSatMonitor 0 3 4 63 0 CQSigImgMonitor 0 127 4 analogMonitor 0 0 aoaFovCfg -1 -90 90 -90 90 cfarFovCfg -1 0 0 60 cfarFovCfg -1 1 -1 1.00 sensorStart
Does anybody have an idea why this is happening?
Thank you