Hello experts,
It means it is difficult to detect the range as below?
- 0~20%RH/80~100%RH with ±0.1% resolution/±3%RH accuracy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello experts,
It means it is difficult to detect the range as below?
- 0~20%RH/80~100%RH with ±0.1% resolution/±3%RH accuracy
Hi Akashi-San,
Thank you for your post. You are correct that condensation makes it impossible to detect humidity properly. Condensation on the sensing polymer will interfere with the humidity readings.
We do not have a maximum temperature accuracy specification for this part below 5 °C, but figure 3 does provide a typical accuracy down to -40 °C.
The part will continue to operate below 0 °C, and between 0 to 100%RH, but RH accuracy is not guaranteed outside the ranges in the datasheet. 100% RH implies that the part will be very likely to be exposed to condensation, and below 0 °C the amount of water that air can hold is extremely small. This makes its difficult for the HDC2080 to accurately detect ambient moisture under those conditions.
Best Regards,
Brandon Fisher
Hello Brandon-san,