Hi TI,
In the document swra549, two corner reflectors are used to do test, the one for indoor measurement has RCS .86 m^2, and the other for outdoor measurement has RCS .11 m^2.
Q1: Are there any reasons to use small RCS for test?
Q2: What will be the issue that I use 100 m^2 RCS (big corner reflector) to do the similar test? I have one 2DFFT result which is from the indoor test. The radar board to the reflector is about 4.5m. The strongest peak is the reflector, and the noise floor is very noisy. Do you have idea what I did wrong for my test?
Thanks,