Hi,
How to generate a .bin file for CANFD driver code and using the same test application code that is released by TI.
SDK ver using:mmwave_sdk_03_03_00_03.
Thanks and regards,
Vijaya Krishna
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
How to generate a .bin file for CANFD driver code and using the same test application code that is released by TI.
SDK ver using:mmwave_sdk_03_03_00_03.
Thanks and regards,
Vijaya Krishna
Please consult the SDK's user guide in the /docs folder. Section 4.5 contains information on setting up the build environment and rebuilding drivers and test code. Building in the SDK is done with makefiles and gmake (gmake is installed with the SDK). If you have modified the CANFD driver and want to rebuild both driver and test code, you will do the following (once the environment is setup)
cd <driver folder>
gmake clean
gmake all
Ah, I see. To generate an executable .bin file, you need to run the Image Creator tools. You will find them in C:\ti\mmwave_sdk_03_04_00_03\packages\scripts\ImageCreator. There is a user guide in that folder as well. In your case, you would only need to create an image with the MSS .xer4f - for a test driver executable, you won't need DSS or BSS firmware images. The command sequence is not too straightforward, so I would also refer you to either the mmw demo's makefiles, or any of the lab's projectspec files in the Automotive or Industrial toolboxes located in the TI Resource Explorer.
-dave