Hello,
Our sensor is using AWR1843 Radar chip, and we notice some target-dependent noise from the 2D FFT plot.
The first and second figure is the FFT of testing in the empty chamber and there is no apparent noise after range bin 120 (120 bin is the end of the chamber room). However, after putting 1 corner reflector (around 90 bin) into the detection area, the 2D FFT becomes noisy as shown in the third figure. Moreover, these noises are located in different Doppler bins as circled in the fourth figure. Two strong noises are on the side of the target, and the other three are in the place that has already exceed the chamber range (ghost targets).
We have been looking this from an SI/PI standpoint and also from a potential front-end saturation standpoint. It would be good to get some guidance from TI engineers and see if others are seeing this same issue.
Looking forward to your replay.
-Simon