• TI Thinks Resolved

LM75A: LM75AIM: About rise time tolerance

Prodigy 30 points

Replies: 8

Views: 72

Part Number: LM75A

Q1:I2C interface electrical characteristic, What is the maximum allowable rise time?

Q2:If SDA and SCL rise time is 3.2usec, is there a problem happen?(SCL frequency is 25kHz)

      Is there any possibility of IC damage?

Q3:When I2C interface receive data,how long it will take from clock judge H to the data latch?

Q4:When I2C interface transmission data, how long it will take from clock judge H to the data output?