Part Number: LDC1101EVM
Other Parts Discussed in Thread: LDC1101
Hi,
I've been testing the noise performance of the LDC1101 EVM, and was wondering if someone could please sanity-check my numbers (they seem high):
Configuration settings:
LDC1101 EVM placed in open-air, no metal targets used for baseline noise assessment.
Ti LDC1101 EVM GUI used in LHR mode to set registers/collect results.
LHR RCOUNT: swept to yield different sampling rates
Clock Divider: 1 (setting clock divider >1 yields significantly better noise SD results,
but application notes say to keep clock divider = 1 when fclk > fsensor_max, which is
always the case for the EVM, with fclk = 12MHz and fsensor_max = 10MHz).
INTB Disable: Donot Report Data Ready
INTB Function: Disabled
RP_Min: 3kOhms - this yielded the best noise performance of the available RPmin settings
Optimize LHR Measurement: Enabled (this disables amplitude adjustment needed for Rp measurement, whic we don't want for LHR measurement)
Sensor FMIN: 2.7MHz - did not affect open-air measurements. This is the sensor frequency at/below which the LDC1101 checks if LC oscillation
has died
All settings were according to recommended LDC1101 settings listed in app note:
https://www.ti.com/lit/ug/snou137/snou137.pdf?ts=1593551064777&ref_url=https%253A%252F%252Fwww.google.com%252F
Results:
SD LHR Counts:
11sps (max RCOUNT): 14.365
1ksps: 725.267
5ksps: 6623.179
10ksps: 8134.653
To calculate the sampling rate wrt RCOUNT, I used:
tconv = (55.0+RCOUNT*16.0)/fclk_in
where fclk_in = 12 MHz
Questions:
1) do my measurements make sense for the LDC1101 EVM? I ask because these numbers are much higher than the standard deviation codes reported in Table 2 for the LDC161x (https://www.ti.com/lit/an/snoa931a/snoa931a.pdf?ts=1591912424026), and I'm wondering what factors could attribute to the differences in performance.
2) For my application, I need <=80 counts SD sampling at 10ksps - should this be achievable with LDC1101 or LDC161x products?
3) In the app note reporting LDC161x performance in Table 2 (https://www.ti.com/lit/an/snoa931a/snoa931a.pdf?ts=1591912424026), was this EVM powered through USB, battery, etc? Could the power source introduce noise into the SD measurement?
4) Are there noise performance advantages of using an external crystal to drive the LDC reference clock, vs. using a microcontroller?
Thanks,
Chris