This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP513: Is there any problem with connecting the Load to VIN+ and the input to VIN- on the TMP513?

Part Number: TMP513

I can see that negative current can be measured, so I assume this is okay, but I wanted to check. I'm measuring a 24V rail. Is it okay, if I connect the 24 rail supply to VIN-, and the load side of the sense resistor to VIN+? I know that this will mean that voltage is measured from my voltage supply to ground (which is what I prefer). And it obviously also means that all positive current will be measured as negative.

I am supplying the sub-regulator with a separate 3.3V supply.