Other Parts Discussed in Thread: AWR2243
Champs, I am working on bringing up the AWR2243 cascade EVM. I am attempting to run a lua script-based demo for use case 1: test source. I have modified the two scripts "Cascade_Configuration_TestSource" and "Cascade_Capture" according to the document "mmwave_studio_cascade_user_guide" from mmwave studio version 02_01_00_00.
I believe I have modified these files correctly. Both scripts run such that the board connects and I believe data is captured. However when I click the "transfer files" button, I receive the error "no of files captured in the directory is zero! nothing to transfer" - This is error is also mentioned in section 8 on page 22. However the language to resolve this error is not clear to me. I have defined a directory. Do i need to create a specific empty bin file to resolve this error? That did not seem to fix it. Can you please let me know what I am not understanding?