hi:
I make a custom pcb, which have a top mmwave board (IWR1642) and a bottom carry board.I use a xds110 probe in the carry board to trasfer data. There is a issue when i run the people conting demo. I can download the peole counting firmware successful ,but when i download the config para, i found it seeems not working. ther are 2 things i cant explain, one is The com_port used to download the firmware and the cfg should is the same one;another is when i migrate the top mmwave board to another bottom carry board(which use a common usb-uart chip to transfer data),it works well,the firmware and the cfg all can be download. So if there is something special with XDS110 probe? how can i download the CFG para?please help!