Part Number: IWR6843
Hi ,
I am running the 68xx_3d_people_counting lab project from mmwave Industrial SDK 4.3.1 after bulding it on CCS verion 9.1.0 and mmwave SDK "mmwave_sdk_03_04_00_03". I cannot able to see the visualiser able to detect the person in front of the sensor nor it is sending any UART logs (neither LED blinks). No changes are done in this project from what was available in the Industrial SDK. Just imported the project and build it.
But while I use the prebuilt binaries from the folder (mmwave_industrial_toolbox_4_3_1\labs\people_counting\68xx_3D_people_counting\prebuilt_binaries) everything is working. Visualiser is able to show the people , it is sending the UART logs and LED is also blinking.
Don't geting what is the problem happening when I build the project and flash it into the board ? Can someone help me resolve this problem.
Thanks and Regards,
Mohit