This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

DRV5055: DRV5055 Z3 and LPG package

Prodigy 10 points

Replies: 1

Views: 38

Part Number: DRV5055

Is the DRV5055 Z3 available in LPG package? I am looking for a linear Hall sensor  with a range of 80-100 mT and sensitivity of 25mV/mT and no temperature compensation, since the magnet I am using is temperature compensated SmCo magnet with 0.001 % / degC reversible temperature coefficient.

Thanks.

  • Sudha,

    DRV5055 Z3 is currently only offered in the DBZ (SOT-23) package.  It is the closest thing that we have to what you are requesting, but then the orientation of the Hall sensor may require a different approach in your system since it is not in the LPG package.

    Another option that may work for your system is TMAG5170 A1.  It offers a digital interface, programmable temperature compensation, and programmable sensitivity with a maximum range of 100 mT. With sensors for all three axes, you should be able to monitor distance regardless of package orientation.

    Thanks,

    Scott 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.