Is there a typo in the TMP461-SP datasheet? "Short-circuit" should be "Open-circuit".
7.3.5 SensorFault
The TMP461-SPdevice can sense a fault at the D+ input resulting from an incorrect diode connection. The TMP461-SP device can also sense an open circuit. Short-circuit conditions return a value of –64°C. The detection circuitry consists of a voltage comparator that trips when the voltage at D+ exceeds(V+)– 0.3 V(typical). The comparator output is continuously checked during a conversion. If a fault is detected, then OPEN(bit 2) in the status register is set to 1.
When not using the remote sensor with the TMP461-SP device, D+ must be connected to D– or GND to prevent meaningless fault warnings.