This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] Which devices are best suited for ambient temperature sensing?

Prodigy 550 points

Replies: 1

Views: 164

What should I consider when choosing a sensor to measure ambient temperature?

  • When designing a system for ambient temperature sensing, it is important to consider layout. The sensor must be isolated from other heat-producing components. Please refer to Ambient Temperature Monitoring for reference designs and recommended devices.
    While all TI devices can be used for ambient temperature sensing, here are some devices to consider:
    • TMP112
      • High accuracy digital temperature sensor
      • Zero calibration required
      • Low power makes it suitable for battery-powered operations
    • TMP116
      • High accuracy, zero calibration digital temperature sensor
      • Suitable RTD replacement
      • Compatible with I2C and SMBus interface

    • LMT01
      • 2-pin digital output temperature sensor
      • Can be converted into two-wire temperature probe (wire length up to 2 meters)

    • TMP235
      • High accuracy analog output temperature sensor
      • Low power consumption
      • Positive slope output of 10 mV/°C from -10°C to 125°C

    • TMP61, TMP63 or TMP64
      • Silicon-based thermistor with a positive temperature coefficient 
      • Fast thermal response time
      • Highly linear; removes need for any linearization circuitry 
      • Minimal calibration required

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.