Part Number: TDC7200EVM
Other Parts Discussed in Thread: MSP-EXP430F5529LP, UNIFLASH
Following the TDC7200EVM user's guide, i attached TDC7200EVM to MSP430 and connected them via cable. But there were 2 problems.
1. At computer's [Device Manager], the USB port must be displayed in the form of TDC7200EVM(COMx), but mine is simply indicated as a USB serial device(COMx). I wonder if this notation is a problem with usb driver recognition.
2. When attempting to connect to the GUI ignoring the notation in (1) Device Manager, the connection failed message appears.
I tried to connect by changing the device type to TDC7200EVM and directly selecting the port suitable for the USB COM number(COM9), but the connection failed message appears again.
Is there any way to solve the connection problem? Any help would be appreciated.