This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DRV5032: Asking for the hall sensor DRV5032 design suggestion

Mastermind 25355 points

Replies: 1

Views: 33

Part Number: DRV5032

Hi team,

If customer will overlap DRV5032FA & DRV5032FD in the board layout (one of the two to mount on the board), could customer connect both of pin3 together?


BR,
SHH

  • Hi SHH,

    For the FD version this will be OUT2 so you can use this pin as you like in your application, for the FA version this is a NC pin meaning there is no internal bond wire. So if you were to just replace the FD version with the FA version in the same layout that would be ok.  

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.