Hi, Staff
Large offset output
The current sensor using the DRV401 has been confirmed to operate in a manner that does not meet the device specifications.
An individual whose output (offset output) is large when the input current is 0 A (about 100 mV) or an individual whose offset output changes each time the power is turned on,
There are some individuals that are not stable, such as those whose offset output changes due to changes in temperature and humidity.
From the DRV401 data sheet, I think that it is a probe driver that creates an excitation waveform with an output operational amplifier as a part that may affect the offset output.
If there are other possible causes for the change in offset, would you like to teach me?
best regards
cafain