Part Number: AWR2243
Hi community member,
Theoretically, how many AWR2243P cascades can be connected at maximum?
For example, is it possible AWR2243P 8pcs cascade connection (24 x TX, 32 x RX anttenas)?
Best regards.
Cruijff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AWR2243
Hi community member,
Theoretically, how many AWR2243P cascades can be connected at maximum?
For example, is it possible AWR2243P 8pcs cascade connection (24 x TX, 32 x RX anttenas)?
Best regards.
Cruijff
Cruijff,
There is no explicit limit.
The only limit is maintaining digital sync trigger and LO delay match and maintaining the LO minimum/maximum input power at each of the LO RX ports. This puts restrictions on PCB routing/cabling mismatch, return loss and insertion loss and external LO amplification. Please see the AWR2243 datasheet for LO input/output power minimums/maximums.
Because the AWR2243 LO has limited output power this restricts entirely passive LO interconnect to somewhere between 4 and 8 devices, depending on the specifics of the PCB routing.
Thank you,
-Randy