Hello team,
I have a question reported from my customer.
Regarding config register(0x1A) read back, the default value is 0x2801 as described on the datasheet.
After a while, 0x2800 is read back when he sent a read command.
The bit0 should be reserved and set to "1", is it possible to be changed to "0" as reported? Or the reserved bit can be overwritten?
Thanks in advance.
S.Sawamoto