Other Parts Discussed in Thread: TDC1000, , TDC1011, TUSS4470
Hello,
I'm designing a fluid level sensing with TDC1000.
So I bought TDC1000-C2000evm for test.
It seems that the EVM-GUI is fixed for 1MHz transducer, so I should change the parameters and hardware components in EVM if I use different freq transducer.
Could you give me some advice how should I change the parameters and components in EVM?
Currently I'm looking TDK's B59070Z0285D121 (285KHz), very thin transducer.
Fluid level : From 0.5cm to 100cm.
Thank you.