This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: Data Extraction and Processing

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: IWR1443

Hi,

Im trying to work on multiple people tracking and I have recorded the IWR1443 sensor output with the help of the mmWave Demo Visualizer, a .DAT file was returned.

I searched through the forum and tried to:

1.  Use the capture_demo.m to process the .DAT file, however there was an error in processing. This might be due to the incompatibility of SDK version (im using the SDK 2.1 which does not have the capture_demo.m)

2.  Record using the mmWave Demo Visualizer Recorder, but it's only compatible to SDK 2.0.

Currently, I would like to know what is recorded in the .DAT file using MATLAB. It would be a great help if you could suggest ways for me to process the .DAT file to get target information such as X, Y, Z, Velocity etc, as I need to perform signal processing such Doppler FFT