Hello, team
I am using AWR 1843BOOST with Medium Range Radar (Lab 007) configuration.
My purpose is to take the detections (TLV) from the RADAR to the booster pins where I can take the data and transfer it over TCP/IP to the client application.
Below mentioned is the approach I have taken:
1) I have removed R136 (AR_MSS_LOGGER) and shorted pin 9 of the J5 connector.
2) I have also removed the R128 (AR_RS232TX) and R129 (AR_RS232RX) and shorted the R169(AR_RS232TX) and R166 (AR_RS232RX) of the J6 connector.
With the above approach, I am assuming that detection data (TLV) should come to the BOOSTER PINS J5 or J6.
And I have the following observations:
Ob1). When I try to read data from pin -9 of J5 (which is connected to AR_MS_Logger), I got some data, there was no magic number (Sent at the starting of every data packet in the header) in the raw data.
Ob2). When I try to read data from AR_RS232TX ( Pin 5 of J6) and AR_RS232RX ( Pin 7 of J6), I don't get any data at all. (both on functional Mode and debug/SOP-2 Mode)
Based on the above observations, I am inferring that the
A) AR_RS232 (Rx/Tx) is used to write only the configuration in the AWR, so this might be the reason I am not getting any Detection Data / Data on the AR_RS232(Rx/Tx) pins. Please correct me if I am wrong.
B) I don’t understand why there was no detection data (magic number) on the J5 connector (AR_MSS_LOGGER) in the AWR1843BOOST. Kindly let me know if I am missing something.
C) Since XDS110 creates two ports on the computer when connected using the serial connecter (J8), I infer that AR_RS232(Rx/Tx) is mapped as “config port” and AR_MSS_LOGGER is mapped as “data port”.
Since now I have depopulated R128 and R129, how the config file would be written if I am using the AR_RS232 RX/TX from the J6 ( Please note that I am using Medium Range Radar lab007).
My final objective is to send/receive both configuration data/Detection Data from J6/J5 over TCP/IP.