Tool/software: Code Composer Studio
Hi all,
I am developing an application based on "lab0007_medium_range_radar" project found in “mmwave_automotive_toolbox_3_0_0”
1. I want to know if the CRT algorithm that is used to improve 'max velocity' in the MRR sub frame is running on both groups (0 and 1) of chirps or only in the second group of slower chirps.
2. Using the MRR80 setup: What is the theoretical max velocity I can achieve using the CRT, for this application?
I see the code in function:
“void MmwDemo_interFrameProcessing(MmwDemo_DSS_DataPathObj *obj, uint8_t subframeIndx)”
in “dss_data_path.c” file.
Thank you,
Claudio