Hello,
How can I configure a chirp so that the ramp end time (=sweep time) is of the order of 1 ms? I get an error message I try to but ADC sample rate less than 2000 ksamples/second. Nether can I grow the number of ADC samples to more than 256. We need to improve the snr in the test, and the mobility of the object is low, so the measurement inteval can be hundreds of milliseconds, and Doppler is not needed.
Jarmo Kivinen
Head of Radio Electronics development.