Replies: 11
Views: 119
Part Number: PGA970
Hello,
my customer facing issues with porting an old CSS project to the latest version. Here are the error messages he got:
It would be great if you can help.
Thanks
Jan
Hello
here are additional infos:
The properties at field 'General - Runtime support library' from previous version 6.2 is not compatible with the installed Version 10.0.
You can see the list in the picture which is installed. How can i install an M0 library for PGA970?
In reply to Eduard Sammereier:
Hello Jan and Eduard,
I recommend using the ARM compiler version 5.2.6 if you are starting with the example firmware. Here is a post that describes how to install an old version of the ARM compiler:
Note you will still have to select the runtime support library file manually, or you can add it to the compiler folder.
Regards,
____________
Scott Cummins
Precision ADC Applications
In reply to Scott Cummins:
Hello Scott,
the list of installable software is empty (see picture). Waht can i do?
Hi Eduard,
If you can't see the ARM compiler tools in the available sites, you may need to manually add it. Click on "Add..." and you can enter this link for the ARM compiler:
GCC ARM Compiler Tools Updates software-dl.ti.com/.../win32 Enabled
at the moment your site is not available....
I would start another thread in the CCS forum to ask about this. I am not sure why the sites are not showing up in your program, and I am not very familiar with dedicated CCS questions. Please reach out to the CCS experts, and they should be able to help you. I will of course be able to help with any PGA970 related questions in the meantime.
is it possible to transfer code to other development tools, for example Keil µVision?
Because of a lot problems here with Code Composer Studio, I must ask this question.
Eduard,
It looks like the list of update sites have been cleared. What exact version of CCS 10 are you using? CCS 10.0.0?
ki
-----------------------------------
Did you read the CCS Forum Guidelines & FAQ? If not, PLEASE read it. If you haven't read it in awhile, please read it again to see if any updates were made.
Having CCS problems? Check out the CCS Troubleshooting Guide
Looking for CCS Training/Documentation? Check out the CCS Resources page
Curious about the status of a bug and know the tracking ID? Track it via the public bug tracking portal
NOTE: When a bug is filed and a tracking ID is provided, the thread may then be suggested as "TI Thinks Resolved". Why? Please read the first FAQ of the CCS Forum Guidelines & FAQ
In reply to Ki:
I want to use the latest version (10.0).
Because of lot of issue during migration from one to another Computer, I want to avoid migration whenever possible...
The old version 6.2 (which work on the old computer) have errors at the new computer, too.
It seems that it could be easier to transfer to other development tools than to upgrade the versions...
KiIt looks like the list of update sites have been cleared.
To resolve this issue, please download the extract the attached zip file:
/cfs-file/__key/communityserver-discussions-components-files/1023/bookmarks.zip
Then follow the steps in section 9.3.1 in the link below:
https://software-dl.ti.com/ccs/esd/documents/users_guide/ccs_troubleshooting.html#no-update-sites-found
Instead of using the zip file referenced in the article (which is for older CCS versions), use the one I attached earlier to this post.