Hello,
my customer facing issues with porting an old CSS project to the latest version. Here are the error messages he got:
It would be great if you can help.
Thanks
Jan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
my customer facing issues with porting an old CSS project to the latest version. Here are the error messages he got:
It would be great if you can help.
Thanks
Jan
Hello Jan and Eduard,
I recommend using the ARM compiler version 5.2.6 if you are starting with the example firmware. Here is a post that describes how to install an old version of the ARM compiler:
Note you will still have to select the runtime support library file manually, or you can add it to the compiler folder.
Regards,
Hi Eduard,
If you can't see the ARM compiler tools in the available sites, you may need to manually add it. Click on "Add..." and you can enter this link for the ARM compiler:
GCC ARM Compiler Tools Updates software-dl.ti.com/.../win32 Enabled
Regards,
Hi Eduard,
I would start another thread in the CCS forum to ask about this. I am not sure why the sites are not showing up in your program, and I am not very familiar with dedicated CCS questions. Please reach out to the CCS experts, and they should be able to help you. I will of course be able to help with any PGA970 related questions in the meantime.
Regards,
Hello Scott,
is it possible to transfer code to other development tools, for example Keil µVision?
Because of a lot problems here with Code Composer Studio, I must ask this question.
Regards,
Eduard,
It looks like the list of update sites have been cleared. What exact version of CCS 10 are you using? CCS 10.0.0?
Thanks
ki
I want to use the latest version (10.0).
Because of lot of issue during migration from one to another Computer, I want to avoid migration whenever possible...
The old version 6.2 (which work on the old computer) have errors at the new computer, too.
It seems that it could be easier to transfer to other development tools than to upgrade the versions...
Ki said:It looks like the list of update sites have been cleared.
To resolve this issue, please download the extract the attached zip file:
/cfs-file/__key/communityserver-discussions-components-files/1023/bookmarks.zip
Then follow the steps in section 9.3.1 in the link below:
Instead of using the zip file referenced in the article (which is for older CCS versions), use the one I attached earlier to this post.
Thanks
ki
I have seen that error, though it has been a long time. The root cause was unfortunately never identified. Please see the below post for more details:
https://e2e.ti.com/support/tools/ccs/f/81/t/745390
If the suggestions in the post do not help, please start a private E2E conversation with me. I can provide a workaround so that you can obtain the v5.2.6 compiler.
Thanks
ki
Hello Jan,
there was no success with all suggestions. Version 10 of Code Composer ist not able to use PGA970 on my pc.
I make here a brake. It seems that it need too much time to wake up the workflow!
I copied the complete path from the old pc to the laptop and moved all links manually. Now it seems to work on the laptop and I can scrap the pc.
Thanks for trying to help.
In future I will try to avoid Code Composer Studio. It seems that is not made for maintanance old software.
Best regards.