Hi, I am testing the SRR lab in a custom AWR1843 board but the GUI does not starts, but the MRR lab works ok. I do the same test with the AWR1843BOOST EVK and both labs runs ok, I am using the original code from tirex, I only have changed the data UART pins for the tests in my custom board
changes in pins respect to awr1843boost evk:
UARTB TX
pin F14 to pin P10
CAN
TX: E14 to F14
RX: D13 to H14
we are not using the TM4C1294NCPDTT3
error detected in custom board: we left the pin SOP1 unconnected
where could I find info about the messages interchange between GUI and awr1843?, I need to understand what are the requirements that need the GUI to send the commands automatically, I also dont understand why the MRR lab works ok but the SRR labs does not works
thanks