Part Number: PGA411-Q1
Hi,
Our settings:
VCCSW - 5V from 2.5A regulator
Mode - 7Vrms
Boost output - 12V (Internal boost mode)
Issues:
1. Series to inductor it is drawing more current - 300mA, but boost output voltage - 12.5V
2. IC is heating up and it is keep on increasing - 100+ deg C ( check via thermal camera)
Images are attached for reference. Please help on these issues.
If possible share concern person email ID we can discuss by sharing other related documents to solve this thing.