I am interested in using an LDC1000 in a small induction heater (~10W power level). Is there any way to drive some power mosfets with the LDC1000 to enable higher coil currents? I'm thinking of something analogous to using a power transistor with an opamp. If I could use the LDC1000, I think I could infer temperature of the object being heated by the measured inductance. If I cannot drive power devices with the LDC1000, is there a way to have a "sense coil" in the same magnetic circuit to monitor impedance while the circuit is being driven by another circuit?