Other Parts Discussed in Thread: FDC1004
Hi David and all
I have used cyindrical capacitive sensor with FDC1004 .
Construction : An alluminium rod is passing from the centre of a aluminum cylinder or pipe. Rod is connected to CIN1 and outer pipe is grounded.
Method: I have not used refrence sensor . instead , I have taken reading in an empty tank and considered it at zero level then take a reading with full tank and save the reading as 100% . supposing probe a linear sensor ,
level % ={ count running - count (empty) } / count(max) - count (min) x 100
reading I got is excellent but counts are not stable. counts are jumping till the 9th and 10th bit.
I have used it in generator tanks . and facing problem that the reading is drifting. Specially during day times it increases and at night it decreases. It seems to be happening like this b/c of temperature.
Also when the generator starts it heats up sensor and reading changes.
Some times without any reason. error is from 1 to 5 % .
Is the active shielding can fix the problem ??? where do I make the active shielding?? over the rod which is passing the centre?? or should I put another cylender over the outer pipe and connect it to shield output. ???
or anyother solution please give .
I have used temp. sensor to compensate in software but the problem is that the response of sensor is much faster that the output of the probe. it worsen the overall response .
IS it possible to impliment OOP on this type of probe sensor. ?? b/c u said in application note that symettry is the key for both parts of sensor.
Kindly give your suggestion to make the sensor accurate and rubust .
With best regards
khalid