This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP102-Q1: Accuracy

Part Number: TMP102-Q1

Dear Support Team;

I have a question about accuracy of TMP102-Q1.

The following value In datasheet.

Maximum accuracy : -20℃ to 85℃ ±2℃

Maximum accuracy : -40℃ to 125℃ ±3℃

How many accuracy at -40℃ to -20℃ and 85℃ to 125℃?

Best Regards,

 Masaaki Sugiyama