Part Number: AWR1642
Hi,
I want to implement a bootloader program.I have some issues:
1.For the AWR1642 , What is the program entry address?
2.I learn about that it can load two problem,If the first program runs incorrectly, the system will automatically load the second program?
3.Falash have four blocks,Which is the backup block,and i want to know the four block's addresses.
4.If bootloader are warning when loading a program after erasure the flash,How to get the program back to normal automatically?
Thanks,