This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3002: different logic voltage from VDD

Part Number: OPT3002
Hi,

My customer want to use OPT3002, but the application has different I/O voltage from VDD as shown in below. Is that no problem? The logic HIGH input voltage (V_IH) is described as 0.7*VDD(min.) to 5.5V(max.) according to the datasheet.

Customer's application:
VDD: 3.3V
I/O: 1.8V
I/F:I2C-Fast(400kHz)
No proximity sensor

Best Regards,
Kazuto